Learn about the Community. Join our Core Community to Get Started

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

Precautions when upgrading MicroNet 100 series to MicroNet 50 series controller

Issue

When a MicroNet 100 series LON controller is upgraded to a MicroNet 50 series LON controller, reference in/out objects and the bindings to the LON SNVT bindings are lost.

Product Line

Satchwell MicroNet

Environment

VisiSat Software version 2.1 Builds 137, 148, 148 SP1, 185 and 196.

Cause

The upgrade process removes various items/objects from the original scheme.

Resolution

Updated June 2019

The MicroNet 50 series range MN350, 450, 550, 650 LCD and Touchscreen have been withdrawn from sale.
The IAC 420, 600 and Touchscreen have now also been withdrawn from sale.
No direct replacement is offered.
Further information on these changes can be found in PA-00495 - Notice of Withdrawal - Satchwell Sigma and PA-00528 - End of Commercialization - Satchwell Sigma.

----------------------------------------------------------------------------------------------------------------------------------------------------------

The upgrade process removes various items/objects from the original bubbleland scheme.

See MicroNet 100 to 50 series upgrade precautions.pdf to view more detailed information.

Tags (6)
Labels (1)
No ratings