Follow along for an enriching discussion with our CEO, Peter Herweck, and industry leaders for a captivating Global Keynote at #InnovationSummit Paris 2024. Watch recording and join the #ImpactMaker movement!️
Niagara-MPX modules Version #13 (Build 39)
SpaceLogic for Niagara Forum
This forum is a place for technical users to share information and collaborate on the integration of SpaceLogic BMS controllers into Niagara BMS.
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Posted: 2021-03-0307:11 PM. Last Modified: 2021-03-0410:57 AM
Niagara-MPX modules Version #13 (Build 39)
A new version of the SmartX engineering Module for Niagara is available for testing and has been posted to the box folder.
The release notes will highlight issues that have been fixed. We are in the process of verifying those fixes and I will update the issue log shortly:
Fixed the issues from issue tracker in the Teams sheet :
136,233,251,252,255,256,227,264,266
136 - Changing the Instance ID number of an Analog Value caused the GUI object to loose its wsAnnotation information and end up at zero zero. The bind were not lost.
233 - During download all, after a error when trying to create object, it keeps trying to write to all the properties.
251 - Auto generated Instance ID
252 - Check all folders for instance ID conflicts
255 - Typo in comment for OnDelay and OffDelay blocks
256 - Units on VAV data object and Room Unit display issues
227 - We want to hide Priority_Array slot in wire sheet for Box Flow objec
264 - Error when adding points in a folder
266 - Bug in OneShot function (still another bug to fix in oneshot)
Two important issues include Schneider Points Manager on Folders under Points Extension and Niagara Guide on target fix.
An addition to this release is a signed version of the modules for 4.9. Use the signed modules and the included certificate if you are using 4.9.
Important Note!! - you need to install the BACnet fix below before you can use this version!
Don't forget, to take advantage of Config folders, you will need a patch for Niagara. The zip file contains the files needed for each version of Niagara. Simply pick the version you need and then replace the existing bacnet-rt.jar with the one in this file. Station restart will be required.