Learn about the Community. Join our Core Community to Get Started

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

Visitor Management in Access Expert V3

Issue

How does Visitor Management work in V3?

Product Line

Access Expert

Environment

  • Hosted
  • Premise
  • Version 3

Cause

No directions on how to configure Visitor Management in V3

Resolution

In order to use Visitor Management in V3, here are the steps to get it configured:

  1. Open up a Chrome browser and enter this url http://ax.accessxpert.com
  2. Once the site comes up, enter the instance name and necessary user credentials
  3. From the AX Header, Select Visitor Management Tab
  4. Select the Kiosk Tab and Enter the visitor's name and email address and click Next to proceed
  5. Enter the person who the Visitor is seeing, system will automatically pull up the person, click on Next
  6. Capture the Photo of the Visitor and Crop accordingly
  7. Sign into the Window and click on Check in to see "Person"
  8. An email will be generated to that person to let them know that they have a Visitor
  9. A badge will be shown on the screen which has the Visitor's Photos and information
  10. Click on the Print Button to Print a badge that can be displayed on the Visitors body
  11. Depending on the printer (eg. Dymo being used), there are some settings that may need to be set for a good picture to be captured and Printed
  12. Choose the right paper source as well as scaling value.  In this case, it is set to 70
  13. Once everything is correct click on the Print button to send to the respective Printer
  14. Attach to the Visitor for duration of the Visit
  15. Upon completion of the Visit, select Check Out and this will Check the Vistor Out of the system
Tags (1)
Labels (1)
No ratings