Learn about the Community. Join our Core Community to Get Started

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

How to determine what version of Microsoft .Net is installed on a workstation pc or server.

Issue

How can I tell what versions of .Net are installed on my PC?  When I look at the Add/Remove programs, the C:\Windows\Microsoft.NET\Framework folder and the system information report I see different versions.

Environment

  • CyberStation
  • Continuum Database Server
  • WebClient
  • MicroSoft Windows
  • Windows XP
  • Windows Vista
  • Windows 2000
  • Windows Server

Cause

When installing Continuum Cyberstation or WebClient it is important to know what version of Microsoft .NET is installed on the workstation PC or server machine. 

It can be difficult to tell which version of MicroSoft .Net are installed on a CyberStation PC, WebClient server or Continuum database server hardware.

Resolution

The following link describes how to determine which versions and service pack levels of the Microsoft .NET Framework are installed.

http://support.microsoft.com/kb/318785

Tags (2)
Labels (1)
No ratings