Issue
XBuilder and Port Forwarding
Product Line
TAC INET, TAC Vista
Environment
I/NET or Vista site
Cause
Desire to know XBuilder and Port Forwarding
Resolution
A Xenta 511/527 can be downloaded:
- On the intranet using the actual 511/527 web address
- Remotely using the public IP address
- Using port forwarding by typing in the :9080 (or whatever ports are assigned) after the web address in the XBuilder project.
You will have to change the http and https ports in the XBuilder project to the remote ports.