Learn about the Community. Join our Core Community to Get Started

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

Send SMS with EcoStruxure Building Operation

Issue

Send an SMS text message when an alarm occurs.

Product Line

EcoStruxure Building Operation

Environment

  • Alarming
  • SMS Text

Cause

Sending an SMS Text message in response to an alarm condition will allow the responsible personnel to react immediately, even if they are not currently at the workstation.

Resolution

EcoStruxure Building Operation does not support direct SMS texting.

One workaround is to use an Email to SMS Test service provider that handles conversion of emails to SMS, as emails are easily created in EcoStruxure Building Operation.

 

If direct SMS functionality is required there are work arounds with 3rd party programs such as SysManSMS via file output options (see Using Sysman alert server with StruxureWare Building Operation).

Note that this third party products such as this are not supported or tested by Schneider Electric.

Tags (2)
Labels (1)
100% helpful (1/1)