Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Learn about the Community. Join our Core Community to Get Started
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

Pelco Control Point Software cannot run on the same PC as I/NET Seven Software

Issue

Can Pelco's Control Point Software run on the same PC as I/NET Seven Software?

Product Line

Pelco, TAC INET

Environment

  • All Windows OS
  • I/NET Seven Software
  • Pelco Control Point Software

Cause

The two software packages are not compatible with each other.

Resolution

Pelco's client software cannot be installed on the same PC that is running TAC I/NET Seven.

See TCON 301 - Chapter 6.

Tags (1)
Labels (2)
No ratings