Learn about the Community. Join our Core Community to Get Started

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 
Announcements
Discover the Exchange Community Top members of July 
Discover the latest features your community has to offer: register to the webinar here

Mobile Apps for Access Expert

Issue

Mobile Apps for Access Expert

Product Line

Access Expert

Environment

Access Expert site desiring the use of modern technology

Cause

Unable to find or know where to look for the Mobile Apps for Access Expert

Resolution

Based on the version of software using Version 2 (V2) or Version 3 (3) the apps are different for each, so please understand the differences. These can be downloaded from the app store on iOS devices. 

For Version 2, there are three Mobile Apps depending on what is needed by the client, these are:

  1. Go to the App Store, click on Search and enter Keep and download the following apps
  2. Keep Monitor - which monitors what is taking place like the events on the system
  3. Keep Notify - which notifies the user via emails and texts if there is an Alarm that has been generated
  4. Keep Personnel - where existing users can be verified or picture updated etc

For Version 3, there is only one Mobile App called Keep Mobile, this gives a general oversight of the system and what is going on with it.

  1. Go to the App Store, click on Search and enter Keep and download the following app
  2. Keep Mobile - which gives you the ability to see all users, events and Hardware that are configured on the system
Labels (1)
100% helpful (1/1)