Learn about the Community. Join our Core Community to Get Started

Schneider Electric Exchange Community

Discuss and solve problems in energy management and automation. Join conversations and share insights on products and solutions. Co-innovate and collaborate with a global network of peers.

Register Now
Knowledge Base
cancel
Showing results for 
Search instead for 
Did you mean: 

Find broken TGML bindings and links in TAC Vista Workstation

Issue

A new feature is introduced in TAC Vista Workstation 5.1.7, enabling the user to identify broken and empty TGML bindings and TGML Links in TAC Vista Workstation. This feature can also list all bindings and links in TAC Vista Workstation, replacing the search function previously used to identify bindings and links in TAC Vista Workstation.

Product Line

TAC Vista

Environment

Vista 5.1.7 and above

Cause

Compiling a list of all bindings, or all empty or broken bindings, allows a user to quickly find and update any graphical problems cross an entire database at once.

Resolution

From Workstation, right click on a folder and choose "Find broken bindings."

This replaces the previous method of searching for broken bindings within the Search window. Note the following object types are no longer available in the TAC Vista Workstation search function:

  • TGML Bindings
  • TGML Dynamics
  • TGML Link
  • TGML Links

See TAC Vista Technical Manual Chapter 28.2 for additional information about this feature.

Tags (3)
Labels (1)
No ratings