EBO Idea Exchange
Have ideas on how to improve the EcoStruxure Building Operation? Please share and get votes from our Community to influence development efforts.
Visit the brand new Software & Firmware Center, within EcoXpert Extranet
What are the main changes vs the previous solution :
For a better user experience and usability, files will be organized by “Software packages” related to versions (ex : EBO 2022).
A package now includes all needed items for the installation of a given version:
User | Likes Count |
---|---|
6 | |
5 | |
4 | |
2 | |
2 |
Hi
Would it be possible to set something up where if you drag an input/output etc from an IO module into bacnet application folder, instead of just creating struxure ware shortcuts, it creates a bacnet point and binds it. Or even just creates the correct type of point. At present we have to create points in an IO and then again in the bacnet application folder. This can be quite time consuming when on the bacnet side as each point has to be created individually.
Thanks Chris
Link copied. Please paste this link to share this article on your social media post.
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.