APC UPS for Home and Office Forum
Support forum to share knowledge about installation and configuration of APC offers including Home Office UPS, Surge Protectors, UTS, software and services.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-06-29 11:06 PM . Last Modified: 2024-03-20 12:54 AM
Hi,
I have both a BK350EI and a BE700G-GK.
Windows 7 x64.
I'm trying to make a VC2008 c++ program detect when the UPS is on battery power.
Is there a way to detect "power off line" status via the existing windows APIs for this purpose. If not - Why not?
Is the only benefit of this device some low sounding beeps that goes of 10 minutes before the power is cut?
i.e a delay of the power cut, but if no one hears the alarm no one hears the beeps there are no benefits at all?
There must be a way to write a program that can detect the power problem - I want to do that using WIN32 and c++...
Have tried two different approaches:
1. fails to detect anything when the UPS plug is removed from the wall.
SYSTEM_POWER_STATUS stPS;
GetSystemPowerStatus(&stPS);
- same info returned both when on battery and when on line power.
2. fails to detect anything when the UPS plug is removed from the wall.
WM_POWERBROADCAST via
hPowerSourceNotify = RegisterPowerSettingNotification( hWnd, &GUID_ACDC_POWER_SOURCE, DEVICE_NOTIFY_WINDOW_HANDLE );
hBatteryPowerNotify = RegisterPowerSettingNotification( hWnd, &GUID_BATTERY_PERCENTAGE_REMAINING, DEVICE_NOTIFY_WINDOW_HANDLE );
- no events are sent when on battery.
The USB cable to the computer should add expected benefits, not confined to the PowerChute software.
How do you access useful info from the UPS device using VC2008 c++ in windows?
Regards
/Ronnie
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-06-29 11:06 PM . Last Modified: 2024-03-20 12:54 AM
Thanks for your reply,
I managed to get it working.
First i tried writing for the HID Power Device spec by using hidapi-0.7.0, and probably it can be made working with more effort...
But I abandoned that and installed the alternate drivers from www.apcupsd.org.
The program apcaccess displayed all the info I could want, and i looked in the source and implemented the status-command via sockets and parsed the text to get what i wanted.
One could parse the output of apcaccess instead, to skip the socket handling.
It seems wrong that such facilities are not made available by APC, you have paid for a product that is crippled by default.
I realize that the registry could be used to monitor (limited) status, but it seems more like a hack.
/Ronnie
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-06-29 11:06 PM . Last Modified: 2024-03-20 12:54 AM
Hi Ronnie,
I've never tried to use VC2008 to monitor a UPS, but here's two approaches I'd attempt:
1) Since the UPS is a standard USB HID Power Device (spec is here), you could try looking at the PowerSummary ACPresent usage.
2) I've also heard that PowerChute maintains several registry keys with useful information. I haven't investigated this, but you might look to see if there's one that shows AC present.
3) You can replace PowerChute's shutdown program with your own like these guys over here.
I think the windows API functions aren't working for you because PowerChute needs to disable windows' built-in UPS support in order to function correctly. Hopefully you can still get the information you need using the above methods, and if not, you can uninstall PowerChute to re-enable Windows' UPS support.
Let us know how you make out.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-06-29 11:06 PM . Last Modified: 2024-03-20 12:54 AM
Thanks for your reply,
I managed to get it working.
First i tried writing for the HID Power Device spec by using hidapi-0.7.0, and probably it can be made working with more effort...
But I abandoned that and installed the alternate drivers from www.apcupsd.org.
The program apcaccess displayed all the info I could want, and i looked in the source and implemented the status-command via sockets and parsed the text to get what i wanted.
One could parse the output of apcaccess instead, to skip the socket handling.
It seems wrong that such facilities are not made available by APC, you have paid for a product that is crippled by default.
I realize that the registry could be used to monitor (limited) status, but it seems more like a hack.
/Ronnie
Link copied. Please paste this link to share this article on your social media post.
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.