Follow along for an enriching discussion with our CEO, Peter Herweck, and industry leaders for a captivating Global Keynote at #InnovationSummit Paris 2024. Watch recording and join the #ImpactMaker movement!️
BACnet Configuration Issues: MSTP Enhanced Mode
EcoStruxure Building Advisor Ideas
Have ideas on how we can improve the EcoStruxure Building Advisor? Please share and get votes from our Community to influence development efforts.
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Send New InviteClose
Announcements
Find the latest Product Announcesments on The Exchange here: PA-00941 - EcoStruxure Building Advisor - New Features Q2 2023
Enhanced Mode is for b3 controllers only. Therefore, there should be a recommendation to change the setting for the following conditions:
If MSTP Comm Port has all b3 controllers, then Enhanced Mode should be TRUE.
If there are no b3 controllers on that MSTP Comm Port, then Enhanced Mode should be FALSE.
If there is a mix of b3 and other BACnet devices, then either position could improve or worsen communications, so it does not need to be included in a recommendation.