Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
79300members
343972posts

Shutting down a vmware cluster

Solved
Spiff_21_apc
Crewman
Crewman
0 Likes
1
81

Shutting down a vmware cluster

This was originally posted on APC forums on 2/3/2012


I want to make sure that our vmware cluster, vill close down correctly, in case our UPS, A smart UPS 30, if it runs out of battery. After reading the guide on how to install PCNS, on a VMA, server i setup this, but found out that it only shuts down the hosts.

My problem is that there is no intrgration with vcenter so you cannot really set a shutdown order. This as i see it can leed to the mass migration away from the first host that is beeing shutdown, over to a second host, that is also in the middle of a shutdown. As i see it this is BAD, and could potential lead to corruption.

Question is how do i correctly setup powercute, or any other program to close down the vmware cluster.

Jakob Lundqvist


Accepted Solutions
david.grehan_at_apcc.com_apc
Crewman
Crewman
0 Likes
0
80

Re: Shutting down a vmware cluster

This was originally posted on APC forums on 6/14/2012


Please see the following KBase article:

http://nam-en.apc.com/app/answers/detail/a_id/11622/kw/HA

See Answer In Context

1 Reply 1
david.grehan_at_apcc.com_apc
Crewman
Crewman
0 Likes
0
81

Re: Shutting down a vmware cluster

This was originally posted on APC forums on 6/14/2012


Please see the following KBase article:

http://nam-en.apc.com/app/answers/detail/a_id/11622/kw/HA