Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
You can subscribe to this forum after you log in or create your free account..
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
Posted: 2021-06-26 03:49 AM
This question was originally posted by Aldar on APC forums on 1/16/2009
Hi,
Could anyone inform me what is the battery pack DC voltage for SU VTP 30K?
Thanks,
Aldar
Posted: 2021-06-26 03:49 AM
This reply was originally posted by Aldar on APC forums on 1/16/2009
Hi,
Could anyone inform me what is the battery pack DC voltage for SU VTP 30K?
Thanks,
Aldar
Posted: 2021-06-26 03:49 AM
This reply was originally posted by Angela on APC forums on 1/22/2009
just a follow up..
it is a common neutral in the system, if you are using dual mains then you must supply 4W plus ground, same as mains input.
Posted: 2021-06-26 03:49 AM
This reply was originally posted by Angela on APC forums on 1/17/2009
i'll have to double check monday but i saw it noted as "split battery referenced to neutral."
i'll follow up monday for you 😉
Posted: 2021-06-26 03:49 AM
This reply was originally posted by Aldar on APC forums on 1/17/2009
Thank you!
+/-192 VDC means there are 2 rows of 192VDC with one common point? Like:
+192 <----------> 0 <---------------> -192
I I I
I I I
I-----------------------I-----------------------I
What confuses me, this common point "0" is also used to wire neutral (N) of second mains (when dual mains are used). Is it right?
Thanks.
Message was edited by: Aldar - corrected "drawing"
Posted: 2021-06-26 03:49 AM
This reply was originally posted by Aldar on APC forums on 1/23/2009
Thank you very much!
Dual mains are not used. Indeed this DC wiring is correct, UPS is now running.
Just for information, the 3 phase input must be wired in some particular order, otherwise UPS gives "wiring fault". Like L2 shifted forward by 120deg comparing to L1.
Regards,
Aldar
User | Count |
---|---|
4835 | |
190 | |
111 | |
108 | |
67 | |
63 |
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.