Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
79240members
343869posts

Lost the local network management interface-to-UPS communication.

Solved
driver111_apc
Crewman
Crewman
0 Likes
2
135

Lost the local network management interface-to-UPS communication.

This was originally posted on APC forums on 11/27/2019


Hi all,

Im having an odd issue where I lose management to the UPS from the NMC when input power is lost, or a run time calibration is started.

Recent Device Events
Date Time Event
11/28/2019 10:06:42 UPS: Lost the local network management interface-to-UPS communication.
11/28/2019 10:06:15 UPS: Runtime Calibration started.


I updated the firmware from 6.2.1 to 6.8.0 but the issue still occurs. There are no other comms plugged in to UPS except network cable.

UPS: SMX750I - 03.8 (ID11)
NMC2: AP9630 - SUMX v6.8.0


Thanks in advance!

Brendan


Accepted Solutions
driver111_apc
Crewman
Crewman
0 Likes
0
136

Re: Lost the local network management interface-to-UPS communication.

This was originally posted on APC forums on 11/28/2019


Hi Frank,

The current 03.8 seems to be the latest version. 

Thanks

See Answer In Context

2 Replies 2
apctux_apc
Crewman
Crewman
0 Likes
0
136

Re: Lost the local network management interface-to-UPS communication.

This was originally posted on APC forums on 11/28/2019


Hi Brendan,

do you also check for an firmware update of the ups device itself?

driver111_apc
Crewman
Crewman
0 Likes
0
137

Re: Lost the local network management interface-to-UPS communication.

This was originally posted on APC forums on 11/28/2019


Hi Frank,

The current 03.8 seems to be the latest version. 

Thanks