Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
You can subscribe to this forum after you log in or create your free account..
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
Posted: 2021-07-01 07:03 AM
This was originally posted on APC forums on 3/6/2015
I upgraded four of our 7901 PDUs to v3.7.4 and for two of them, all of the data under the first menu choice "Device Manager" are missing.
Posted: 2021-07-01 07:03 AM
This was originally posted on APC forums on 3/6/2015
Ok. You have gibberish for the application string, and the app is not running properly (the "A-") in the Stat: section.
What is a little confusing is that it says it has been up for 15+ days, yet you said you just upgraded it? I would suggest re-running the upgrade utility and see if it clears things up.
Posted: 2021-07-01 07:03 AM
This was originally posted on APC forums on 3/6/2015
Right after you log in, do you see the bolded text below:
American Power Conversion Network Management Card AOS v3.7.4
(c) Copyright 2009 All Rights Reserved Rack PDU APP v3.7.4
Switched Rack PDU: Communication Established
If not, can you post what you do see there?
Edit - for some reason, although I see bold text in the preview, it doesn't show up in the post. The parts I am talking about are "Rack PDU APP v3.7.4" and "Switched Rack PDU: Communication Established".
Posted: 2021-07-01 07:03 AM
This was originally posted on APC forums on 3/6/2015
Here is the output of one of the units that is having problems
BAD UNIT
American Power Conversion Network Management Card AOS v3.7.4
(c) Copyright 2009 All Rights Reserved F~PW~~~~~~~~~V~~F~;V~uQ;F~uL~F~F~~V~~F~~F~~V~~F~3~ v~.~.V.~
-------------------------------------------------------------------------------
Name : SWPL-R01PDU02 Date : 03/06/2015
Contact : SW-Cloud0IT@steelwedge.com Time : 14:12:03
Location : Pleasanton, CA User : Administrator
Up Time : 15 Days 18 Hours 33 Minutes Stat : P+ N+ A-
------- Control Console -------------------------------------------------------
1- Device Manager
2- Network
3- System
4- Logout
> 1
------- Device Manager --------------------------------------------------------
>
Posted: 2021-07-01 07:03 AM
This was originally posted on APC forums on 3/6/2015
Ok. You have gibberish for the application string, and the app is not running properly (the "A-") in the Stat: section.
What is a little confusing is that it says it has been up for 15+ days, yet you said you just upgraded it? I would suggest re-running the upgrade utility and see if it clears things up.
User | Count |
---|---|
4834 | |
190 | |
111 | |
108 | |
67 | |
63 |
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.