Remote Operations Forum
Support forum for Schneider Electric SCADA systems, radios and RTUs. From commissioning integration devices and software, to enhancing existing installations or troubleshooting.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-08-06 05:45 AM
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-08-06 08:39 PM
It's been a little while since I last set this up, but I don't remember it being too tricky.
What is your IP subnetting plan?
If you have two radios, then you need three subnets.
1. Radio WAN
2. Radio #1 LAN
3. Radio #2 LAN
and you will need to setup the IP addresses for both the LAN and WAN of each radio correctly for the subnets.
Then set up some routes.
Radio #1
1. Radio #2 LAN should go via Radio #2 WAN IP
2. Radio #1 likely needs a default route outbound also (through LAN router etc)
Radio #2
1. Radio #1 LAN should go via Radio #1 WAN IP
2. if you want default routes, then this would also need to go via Radio #1 WAN IP (unless Radio #2 will also have an outbound connection available from its own LAN)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-08-09 08:59 AM . Last Modified: 2021-08-09 09:03 AM
Having a mix of Gen I and Gen II radios should not be a concern for your system. The primary differences on the newer radio are the physical size, the added (optional) Rx-only port, and the two digital I/O points. The Gen I radios will take the same firmware and configuration as Gen II.
We have a series of instructional videos on the Schneider Electric Youtube channel. This one may be most appropriate:
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-08-06 08:39 PM
It's been a little while since I last set this up, but I don't remember it being too tricky.
What is your IP subnetting plan?
If you have two radios, then you need three subnets.
1. Radio WAN
2. Radio #1 LAN
3. Radio #2 LAN
and you will need to setup the IP addresses for both the LAN and WAN of each radio correctly for the subnets.
Then set up some routes.
Radio #1
1. Radio #2 LAN should go via Radio #2 WAN IP
2. Radio #1 likely needs a default route outbound also (through LAN router etc)
Radio #2
1. Radio #1 LAN should go via Radio #1 WAN IP
2. if you want default routes, then this would also need to go via Radio #1 WAN IP (unless Radio #2 will also have an outbound connection available from its own LAN)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-08-09 06:55 AM
Thanks for this I will try this config with my client,
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-08-09 08:59 AM . Last Modified: 2021-08-09 09:03 AM
Having a mix of Gen I and Gen II radios should not be a concern for your system. The primary differences on the newer radio are the physical size, the added (optional) Rx-only port, and the two digital I/O points. The Gen I radios will take the same firmware and configuration as Gen II.
We have a series of instructional videos on the Schneider Electric Youtube channel. This one may be most appropriate:
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-08-10 10:30 PM
Thanks so much for this.
How would we set this up on GeoSCADA though? – Should I set the Q Channel address type to Network rather than TCP/IP under the radio connection Tab?
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-08-11 08:10 AM
In IP Routing mode you will specify the LAN IP address of each remote device you wish to communicate with, and the radios will route the message using the routing rules. With Geo SCADA, as you most likely have multiple remote devices to communicate with, you will set the channel connection type to Network. Then, as you add each remote device (eg RTU or PLC, or even a radio for its own diagnostic information), you will specify its IP address on the Network tab of that outstation.
For more detailed assistance with Geo SCADA, I suggest you post those questions in the Geo SCADA forum on this same website. The group there is very active and knowledgeable.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-08-11 09:42 AM
Thank you, I'm implementing with my client tomorrow I will pass through feedback.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-08-11 10:09 PM
If using a radio as a gateway into a radio network, it can get a little tricky.
You have a few options:
1. Use the radio as the default gateway for the operating system running your GeoSCADA Expert server, and then all packets for remote networks (i.e. your telemetry sites) will go via that radio. This is normally not desired however, since you will already have an IT administered gateway device.
2. Configure some static routes in the operating system running your GeoSCADA Expert server. These static routes should be such that you can reach your telemetry sites via the radio gateway.
Setting up your IP subnets is the most difficult part. If you get it wrong, you will suffer for a long time with having to make complicated and numerous static routes.
Generally the easiest approach is to cut out an entire high level subnet for telemetry. i.e. 10.1.x.x\16
Then you can have something like 10.1.0.x\24 as being your radio WAN subnet... and you'd have room for 254 sites.
Site #1 would be 10.1.1.x\24, the radio on this site would be LAN 10.1.1.1, and WAN 10.1.0.1
Site #254 would be 10.1.254.x\24, the radio on this site would be LAN 10.1.254.1, and WAN 10.1.0.254
If you need more sites, but have less things on each site, then you can use smaller subnets than \24
I've got a customer that uses \28 for radio sites, which allows for 13 devices (+radio), normally that's more than enough... but I find my brain handles the maths better if I use nice full \n*8 subnets
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-08-12 06:23 AM
Thanks so much, I was to solve the issues faced and was able to communictae to GeoSCADA.
Thanks
Link copied. Please paste this link to share this article on your social media post.
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.