Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
80734members
346702posts

SCADAPack 474 Increase Event Buffer

Teaan
Lieutenant JG
Lieutenant JG
0 Likes
0
167

SCADAPack 474 Increase Event Buffer

Hi,

 

I am using a SCADAPack that is reading close to a 1000 tags from a PLC over Modbus that must be communicated to SCADA over DNP3. 3G/GPRS communication is used which can at times fail for 3+ days. Currenlty I have set the event buffer to maximum size of 40000, which basically allows for 40 events per IO before buffer overflow occurs. Is there anyway to store events for longer periods of time if such a failure occurs?

 

Regards

Teaan