Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
79287members
343963posts

SCADA (Oil Pipeline) support needed

MSD
Crewman
Crewman
0 Likes
1
177

SCADA (Oil Pipeline) support needed

Dear Experts,

 

I don’t have much knowledge on SCADA system and now working for a new project of cross-country Oil transportation pipeline SCADA. It’s a pipeline of more than 200 Km with 2 terminals (dispatch & receiving) and several valve stations through the pipeline will be connected with the central SCADA. The communication will be done by OFC placed along the pipeline. Apps of Leak detection system (LSD) have to supply and integrated with the SCADA system.

 

Please suggest me if there any suitable & efficient SCADA software of Schneider for oil transportation pipeline SCADA with leak detection system.

 

Thanks

1 Reply 1
sbeadle
Janeway Janeway
Janeway

Re: SCADA (Oil Pipeline) support needed

Hi,

Geo SCADA Expert has been used in many pipeline projects worldwide.

https://shop.exchange.se.com/en-US/apps/69629/ecostruxure-geo-scada-expert

https://community.exchange.se.com/t5/Geo-SCADA-Knowledge-Base/bg-p/geo-scada-knowledge-base

https://www.youtube.com/watch?v=5wZl-tHuFkg&list=PLa7UGrWOTyjnPpCJxnTZkdBM_6D70qoKl&index=14

LDS apps can use OPC to communicate with Geo SCADA Expert.

Please talk to your SE local representative for Telemetry and Remote SCADA.

Best regards

Steve