Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
79476members
344260posts

New version of Realflo Flow Computer (7.02.1) now available for download from Exchange SHOP

MartinChartrand
Commander Commander
Commander
0 Likes
1
482

New version of Realflo Flow Computer (7.02.1) now available for download from Exchange SHOP

Hello SCADA & Telemetry Community,


Realflo 7.02.1, the multi-run flow computer is available for download from SHOP.

 

Realflo is a software solution that works in tandem with standard SCADAPack and latest-generation SCADAPack x70 Smart RTUs to provide gas and liquids flow measurement for well test, allocation measurement, production optimization, and well pad control.

 

Version 7.02.1 adds the following new features to Realflo's already powerful and flexible tool set:

 

  • AGA-9 gas flow calculation for ultrasonic meters is provided on SCADAPack 57x and 47x RTUs, and on SCADAPack 300 series RTUs.
  • AGA-8 (2017) density calculation is provided on SCADAPack 57x and 47x RTUs, and on SCADAPack 300 series RTUs. The following calculations are now provided: AGA-8 Detail (1994), AGA-8 Detail (2017) and AGA-8 GERG (2017)


Please access Realflo 7.02.1 from SHOP using this link: <click here> 

 

Thank you.

Martin Chartrand

1 Reply 1
S_Stolyarov
Lieutenant
Lieutenant
0 Likes
0
423

Re: New version of Realflo Flow Computer (7.02.1) now available for download from Exchange SHOP

Good news, Thank you for the information!