Follow along for an enriching discussion with our CEO, Peter Herweck, and industry leaders for a captivating Global Keynote at #InnovationSummit Paris 2024. Watch recording and join the #ImpactMaker movement!️
M580 Explicit Messaging with Simocode EIP
Modicon PAC Forum
A forum for topics related to the scope of Modicon PAC offers and ecosystem along the whole lifecycle: Modicon M580 and 340, EcoStruxure Control Expert, EcoStruxure Process Expert (Unity Pro) and more.
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Posted: 2021-09-1406:34 AM
M580 Explicit Messaging with Simocode EIP
HI Community,
I am trying to do Ethernet/IP Explicit Messaging using Data_Exch Block to read Acyclic Data from Siemens Simocode ProV EIP.
First the Structure of Send_Req Pin is not Clear, what are Class Segments, Instance Segments and Attribute Segments. I have made Array of INT type and given Request size & Service Code INT[0] , Class INT[1], Instance INT[2] and Attribute in INT[3].
Addressing is done using ADDMX block.
Plus for Management Tag[3], setting length as 8 bytes. Management Activity Bit 0.0 is not toggling but the activity counter in Byte 1 is continously changing. there's no error code in Management INT[1] probably because Activity Bit is not toggling.
RECP is Array of INT Type, First INT element is Showing code 16#048E.
Above application is Get_attribute_Single but will need to do Get_Attribute_All, Get_attribute_Single and Set_Attribute_Single as well.
I have used this device with Rockwell Clx controller and did Explicit messaging there. Need to do the same for M580 too. Please consider me a relative Novice in M580 and respond appropriately as soon as possible.