The LayoutFAST User Group is a place where Specifiers, Contractors, and Panel Builders share their User experience with the tool and ask Schneider Electric experts questions to solve their issues.
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Posted: 2023-06-2809:28 AM
QED 2 dimensional discrepancies
QED2 switchgear dept discrepancies is huge and it is not acceptable. if the gear doesn't match the dimensional information how it is expected to be sent or used by customers?
In the attached pictures there is 3 sections one section is can be set at 71.5" deep the other 2 section cannot. second section can be only 60" and third section is only 47.5" deep, why?
The actual dept form factory is 71.5" deep.
How are these models are if they are so different?
What's the point of using them if they cannot be modified?
Also can anybody elaborate on this message?
"Error in updating the family symbol: Document.Create canonly be used with project documents. use Document.FamilyCreate in the Family Editor."