Hi,
We very recently deployed 2 x DCE Basic on a project. The 2 are monitoring 2 separate Prefabs. For some reason, one of these servers had a message "Memory is detected, but not configurable on the display in orange.
During testing, one of the tests was to record boot time of the servers and the server could not boot up.
When connecting a monitor to the server it come up with a critical memory error "An error was detected during memory initialization. Verify the DIMMs are properly seated and that they are installed in the correct sockets."
A hard reboot resolved the issue but am certian that they issue will be back at some point. I picked up the below in a Dell forum but would like to know if this is a known issue and if it might also affect the Standard and Enterprise server offerings.