Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
73745members
331055posts

Available  Firmware updates through Eco Struxure IT Management

Rodocola
Crewman
Crewman

Available  Firmware updates through Eco Struxure IT Management

SUMX v696, AOS v696 shows 3 devices out of date => Version APP sumx v6.8.0, AOS v6.8.2, 

RPDU2G v696, AOS v696 shows 4 devices out of date => APP rpdu2g v6.8.0, AOS v6.8.2

 

Question: If I choose to do the updates all of devices is it going to impact the connected load or is it going to trigger alarms due to power loss or restart? Or is it simply will restart the NIC card and not the UPS it self?

 

Sorry if someone all ready ask this question I am very green on the UPS department.

 

Thank you in advance 

Attachments
Tags (1)
1 Reply 1
JLehr
Lt. Commander Lt. Commander
Lt. Commander

Re: Available  Firmware updates through Eco Struxure IT Management

Hi @Rodocola,

 

Have a look at this article in the EcoStruxure IT help center. It states: 

 

Tags (1)