Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
You can subscribe to this forum after you log in or create your free account..
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
Posted: 2022-01-18 08:08 AM
I have installed GeoSCADA Expert 2021 (6.84.8027.1) - Initial Release
For some reason the special theme you can add to ViewX is no longer working.
Registry “Computer\HKEY_LOCAL_MACHINE\SOFTWARE\WOW6432Node\Schneider Electric\ClearSCADA\ViewX\ViewXThemeName= MetroWhitePurple”
Now I have to deal with the annoying Schneider green.
Is this changed for 2021 release?
Posted: 2022-01-18 11:00 AM . Last Modified: 2022-01-19 04:15 AM
The ViewX theme feature is no longer available in Geo SCADA Expert 2021.
I believe this is related to the new version 21.1 of the Actipro WPF Controls that ViewX is using.
Correction: Themes are still available, but its a different selection of themes, see Theme names.
Posted: 2022-01-18 02:26 PM
Thanks for replying! Unfortunate - I preferred the "MetroLight" options. Hopefully one day that functionality will return, I personally don't care for the lack of delineation between these menu components at the top:
Posted: 2022-01-19 03:07 AM
@AndrewScott are you sure it's related to the Actipro changes and not to the AVEVA Telemetry Server changes?
Since ATS appears to utilise exactly the same window frames etc as ViewX, but in a blue colour.
It's almost as though the custom colouring has been withdrawn to ensure that the ATS platform can be coloured AVEVA blue whilst the ViewX platform is Schneider green
🙁
Posted: 2022-01-19 03:16 AM
Sorry that was not the answer Bevan!
I'm chasing this up.
In the mean time - try using the colour theme OfficeWhitePurple
Steve
Posted: 2022-01-19 03:46 AM . Last Modified: 2022-01-19 01:35 PM
Ahhh... so perhaps this is the reference to use?
Posted: 2022-01-19 03:51 AM
I perhaps got a little bit too excited at the prospect of a 'Dark' theme... alas it's not quite ready for primetime 😉
Still... there's not huge amounts of theme-capable dialogs to fix.
The property panes would hopefully be pretty quick wins on that front also.
I'll put together a bit of a list of the items still lacking theme support and send it to support tomorrow.
Posted: 2022-01-19 04:18 AM
@BevanWeiss ATS 2019 (6.81) and ATS 2020 (6.82) used the "MetroLightBlue" theme to get the blue colour scheme, but in the upcoming ATS 2020 R2 (6.84) the named theme is no longer used to get the blue colour scheme.
Posted: 2022-01-19 07:24 AM
Thanks; using the "OfficeWhitePurple" theme now.
User | Count |
---|---|
193 | |
78 | |
32 | |
23 | |
18 | |
11 |
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.