Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
79189members
343723posts

C Bus WSiser2_5918 Installation

Datagate-Cochin
Crewman
Crewman

C Bus WSiser2_5918 Installation

Dear Sir,

 

We are facing problem with C Bus Wiser2_5918 installation, Customer has set up static ip in Router. Bust unable to remote access C Bus thru Laptop or Android Mobile. We have set up port forwarding in PICED as well as in Router. Also installed and configured Wiser App in Android mobile. On trying to access it shown Adobe Flash Player emblem and stops there. 

 

However it is working fine within the customer premise thru WiFi.

 

Customer needs remote aceess either thru Laptop and/or Android Mobile.

Regards

R Sreekumar

Datagate

Cochin 20,

Kerala, India

+91 9447046900

Tags (1)
1 Reply 1
Omaelk
Administrator Administrator
Administrator
0 Likes
0
188

Re: C Bus WSiser2_5918 Installation

@sesa122674_brid , could you please support? 

Tags (1)