Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
80833members
346908posts

Smart UPS SRVS1KI battery current is always zero

evrenyeni
Cadet
0 Likes
0
126

Smart UPS SRVS1KI battery current is always zero

Hi folks,

 

I have just gotten a new Schneider SRVS1KI (identical with APC SRV1KI). It works well so far and keeps my system for a decent duration but one thing got my attention: Battery Current is always shown as zero at the monitoring software. I did a full battery discharge test and nothing went wrong.

 

Why it is shown as zero, any ideas? And could the product (or only the battery inside) be defective? Should I send it to the repair center?Main Status Screen during line mode.Main Status Screen during line mode.UPS Info Screen. Battery current is shown as zero here too.UPS Info Screen. Battery current is shown as zero here too.Battery Current Diagram: Always zero :)Battery Current Diagram: Always zero 🙂Self Test Screen: Self test passedSelf Test Screen: Self test passedMain Status Screen during battery test mode.Main Status Screen during battery test mode.

Tags (1)