ubuntu 21.2
apcupsd
UPS:
SRT 10K RMXLI
Smart-USB SRT 10000
We have trouble to make apcupsd to communicate with our UPS, STR 10000 over Ethernet.
On a host machine we have Ubuntu 21.1, impish with latest apcupsd installed.
https is used to manage the UPS web-ui, the UPS web-ui is accessible from the host machine.
Any ideas why apcupsd is not able to get in touch with the UPS?
Do we have to add the host machine's ip address in the UPS web-ui somewhere?
Should "Required authentication cookie" be off?
Regards
"error" message from apctest
>apctest
...
...
Setting up Port
apctest FATAL ERROR in apctest.c at line 319
Unable to open UPS device.
The configuration file for apcups look like this
UPSTYPE pcnet
DEVICE 10.0.0.10:readonly:<long password>
UPS: Smart-UPS STR 10000, UPS is from late last year, firmware is 12.0
Configuration -> Security -> local users -> management
user: readonly
is enabled
type set to "readonly"
password is longer than 15 characters
Configuration -> network -> web access
http is off
https is on
Required authentication cookie is on
Configuration -> Security -> remote users -> authentication
"Local Authentication only" is selected
No configured RADIUS server have been added
Configuration -> Security -> local users -> RADIUS
Two "servers exists" with IP address 0.0.0.0, it is not possible to add more