Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
80874members
346972posts

SMX1500RM2UC fan

lunadesign_apc
Crewman
Crewman
0 Likes
1
171

SMX1500RM2UC fan

Is it true the fan on the newer SMX1500RM2UC units is always on?

 

If true, how noisy is it?

 

Thanks!

Tags (1)
1 Reply 1
JonPro
Ensign Ensign
Ensign
0 Likes
0
83

Re: SMX1500RM2UC fan

@lunadesign_apc,

 

The SMX models use a variable speed fan and the speed is determined by multiple factors such as operating temperature, mode of operation, and load. This operation may vary depending on the model and firmware revision of the UPS.

 

We do not have the date for the fan noise but the acoustic level of this unit is 40 dBA.

 

Please refer to the following links:

Regards,

JonPro
Secure Power Team
Tags (1)