Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
80813members
346879posts

PowerChute Business Edition - Disable forced shutdown

alpha232
Cadet

PowerChute Business Edition - Disable forced shutdown

PCBE version 10.0.5.301 on Windows 10 Home

UPS Smart-UPS SC450 RM

 

 

I am using the UPS to run a rack of networking gear, it does not require time to shut down, and I'm using the UPS solely for extended runtime during outages or when performing some power maintenance. The device that performs the monitoring and other administrative tasks is a laptop and has it's own battery. 

 

I've disabled all available options I am aware of to prevent the PCBE agent from shutting down the computer, however, during runtime tests, it will indeed shut down the computer, I get an alert saying that the agent is shutting down the computer, and there is no quick or easy way to abort it.

 

Any ideas where I've gone wrong or is the software just a problem? 

 

powerchuteeventsettings.PNGpowerchuteshutdownsettings.PNG

 

 

 
Tags (1)
1 Reply 1
BillP
Administrator Administrator
Administrator
0 Likes
0
115

Re: PowerChute Business Edition - Disable forced shutdown

@alpha232 

 

Please read the Note: listed at the bottom of the Shutdown Settings page screenshot you attached. 

 

If you would like to cancel the shutdown once, PowerChute has issued the command open a command prompt as an administrator and enter shutdown /a   

 

See Microsoft doc for assistance with the shutdown command https://docs.microsoft.com/en-us/windows-server/administration/windows-commands/shutdown

Tags (1)