I have TXB-N , D5220 and SPECTRA IV-IP models. I have ONVIF device manager 2.2.250 but the only one which gets Absolute move interface is the D5220. The TXB-N brings only the "Continuos Move" window. Is this because only the D5220 model is compatible…View more
Posted by: rdiaz_1 in Archives: Industrial Automation and Control
Find more articles tagged with: