Invite a Co-worker

Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
55502members
253251posts

SmartConnector SNMP Extension

SmartConnector SNMP Extension

Comfort Laboratory
SmartConnector SNMP Extension
SmartConnector SNMP Extension allows EBO users, to monitor network devices via Simple Network Management Protocol (SNMP). It fits for really big projects! It was tested on up to 20.000 SNMP/EWS server variables capacity! This software is an SNMP manager that obtains data from all required agents (servers) and includes a useful configurator, which allows creating the required configuration quickly. SmartConnector SNMP Extension can be plugged into Schneider Electric SmartConnector Framework as an extension. SNMP Extension allows communicating between SNMP agents and EWS servers, corresponding to user-provided configuration. EWS server generates EBO alarms when TRAP-messages received. This extension supports the following versions of the SNMP protocol: v1, v2, v3. SmartConnector SNMP Extension requires SmartConnector framework version 2.3. and above. Please note that you will need a commercial license for SmartConnector from Schneider Electric.
0 topics and 0 replies mentioned SmartConnector SNMP Extension View all 0
Comfort Laboratory
SmartConnector SNMP Extension
SmartConnector SNMP Extension allows EBO users, to monitor network devices via Simple Network Management Protocol (SNMP). It fits for really big projects! It was tested on up to 20.000 SNMP/EWS server variables capacity! This software is an SNMP manager that obtains data from all required agents (servers) and includes a useful configurator, which allows creating the required configuration quickly. SmartConnector SNMP Extension can be plugged into Schneider Electric SmartConnector Framework as an extension. SNMP Extension allows communicating between SNMP agents and EWS servers, corresponding to user-provided configuration. EWS server generates EBO alarms when TRAP-messages received. This extension supports the following versions of the SNMP protocol: v1, v2, v3. SmartConnector SNMP Extension requires SmartConnector framework version 2.3. and above. Please note that you will need a commercial license for SmartConnector from Schneider Electric.
0 topics and 0 replies mentioned SmartConnector SNMP Extension View all 0
Sort by:
Sort by:

No content available