Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
73887members
331342posts

EcoStruxure™ Plant Builder 5.0

Schneider Electric
EcoStruxure™ Plant Builder 5.0
Speed up EcoStruxure™ Plant Pre-Sales project quotation. The EcoStruxure Plant Builder is a quotation pre-sales tool that satisfies the needs of each player in the solution selling process. It is a standalone tool that is always in line with the latest release of EcoStruxure Plant catalog. Starting from a project specification, the tool proposes and validates a system configuration comprising: - PAC modules - devices - network - software It provides the complete BOM (Bill Of Material) of the full porject with pricing for project bidding, a customized system architecture drawing and a project quotation report.
Schneider Electric
EcoStruxure™ Plant Builder 5.0
Speed up EcoStruxure™ Plant Pre-Sales project quotation. The EcoStruxure Plant Builder is a quotation pre-sales tool that satisfies the needs of each player in the solution selling process. It is a standalone tool that is always in line with the latest release of EcoStruxure Plant catalog. Starting from a project specification, the tool proposes and validates a system configuration comprising: - PAC modules - devices - network - software It provides the complete BOM (Bill Of Material) of the full porject with pricing for project bidding, a customized system architecture drawing and a project quotation report.