Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
73762members
331085posts

LR65 (80 GHz)

Schneider Electric
LR65 (80 GHz)
The new LR64 and LR65 from Schneider Electric offer customers the benefit of reliable, trouble free solids level measurement. Following an easy start-up procedure, the radars use powerful Frequency Modulated Continuous Wave (FMCW) radar technology and advanced signal processing and algorithms to maintain accuracy. A rugged design allows both models to be used in applications featuring: product buildup, sloping material, uneven surfaces, “rat-holes” and other challenges.
Schneider Electric
LR65 (80 GHz)
The new LR64 and LR65 from Schneider Electric offer customers the benefit of reliable, trouble free solids level measurement. Following an easy start-up procedure, the radars use powerful Frequency Modulated Continuous Wave (FMCW) radar technology and advanced signal processing and algorithms to maintain accuracy. A rugged design allows both models to be used in applications featuring: product buildup, sloping material, uneven surfaces, “rat-holes” and other challenges.
Sort by:
Sort by:
Jeff_Blair
Level and Pressure Instrumentation Forum

Posted by: Jeff_Blair 2020-05-05

. Latest Post: 2020-05-06 by qwilliam

2
1390
Related Posts