Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
79301members
343972posts

PME 2021 Cumulative Update 1 is now released!

Michael_Neas
Ensign Ensign
Ensign
0 Likes
2
584

PME 2021 Cumulative Update 1 is now released!

Cumulative Update 1 (CU1) has been released for EcoStruxure Power Monitoring Expert (PME) 2021.

 

PME 2021 CU1 has a number of quality improvements, such as

  • Fixed an issue where Show Advanced option under Measurements dialog in gadgets was missing
  • Fixed an issue breaker configuration tool prevented configuration duplication without Administrator rights
  • Fixed an issue VIP Modbus Slave module didn't connection sessions per configured connections
  • Improved log in performance for standard and Windows users

 

PME 2021 CU1 also comes with following new features

  • More breaker ranges in Breaker Performance Module
    • Masterpact NW ANSI range with NW60H3 designation
    • Powerpact range with RL1000 and RL1200 designation
  • Driver support for Compact NSZ and Powerpact H-, J- and L frame devices
  • Support of TOU in Measurement Statistics Report

 

You will find PME 2021 Cumulative Update 1 and its release note here

 

We highly recommend you apply CU1 to your PME 2021 system.  If you have EcoStruxure Power Operation 2021 with Advanced Reports and Dashboards module, you can also apply PME 2021 CU1 to your Advanced Reports and Dashboards module.

Tags (1)
2 Replies 2
sesa510609_brid
Crewman Crewman
Crewman
0 Likes
1
467

Re: PME 2021 Cumulative Update 1 is now released!

Could someone please verify the link to download PME2021 CU1 is correct?  It is 5 GB ISO.  When I extracted the ISO, it is Power Manager installation DVD..

 

thanks,

 

Hung

Tags (1)
Michael_Neas
Ensign Ensign
Ensign
0 Likes
0
462

Re: PME 2021 Cumulative Update 1 is now released!

Hello Hung,

 

 

When I click on the link both logged in as myself and not logged in at all, it is taking me to the correct box site.  Is this the website that it takes you to:

BoxCU1.PNG

Please feel free to email me direct at michael.neas@se.com and I'll make sure we get you the correct files.

 

Tags (1)