Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
73656members
330843posts

Considerations for electricians working on educational sites

VictoriaSwift
Lieutenant JG Lieutenant JG
Lieutenant JG
0 Likes
2
402

Considerations for electricians working on educational sites

School.jpg

 

Schools. colleges and universities have a very specific set of requirements, with safety and longevity being paramount - so it’s crucial that the right electrical decisions are made, from design through to implementation.

 

During holiday periods when facility managers look to get refits and refurbs carried out, pressure will be placed on electrical contractors to deliver jobs on time and make good long term decisions.

 

There are some key considerations to take into account:

 

Composition

 

With dense, diverse and intermingling populations of students, it’s no secret that educational sites are a breeding ground for germs. For school refurbs, antimicrobial materials are a clear first choice. Electricians should consider their use on surfaces that are regularly touched or in dirt-collecting areas, such as light switches and wiring.

 

Products with antimicrobial qualities prevent the spread of germs, protecting against harmful bacteria such as MRSA and Salmonella. Although there are many antimicrobial coatings and covers on the market, it is important to select products which are inherently protective - where the protection is within the material itself, not just on the surface. That way it cannot be damaged or scuffed, which is essential for a long-lasting refit.

 

Distribution

 

Placement of switches, sockets and wiring cannot be an afterthought. Their positioning has to tick a number of boxes and be considered in terms of accessibility and usability. To comply with Part M of the Building Regulations, electricians must also be considerate of the placement of switches and sockets in a public space.

 

Here are a couple of key points to consider:

 

- Height and freedom from obstruction: accessories and contact points should be installed at a height that makes them accessible but prevents damage from moisture or contact

- Mounting position: sockets should be no nearer than 350mm to a corner, and light switches should align with door handles

 

Application

 

When planning a new job, the end user's needs have to remain the focus. In the case of an educational site with so many different users, steps should be taken to ensure safety and clarity is built into design.

 

Critical and essential supply must also be made easily identifiable. This can include pull cord alarms in toilets, or switches and sockets for special electrical applications such as critical power and security. Use red wiring and accessories to indicate special or emergency use and distinguish from normal use accessories. Additionally, the use of engraved switches and control points should be considered to provide assistance with identifying their purpose.

 

Management

 

For an educational site job, electricians should prioritise a complete solution that provides visibility to the facility manager. Selecting connected technology like Schneider Electric's Acti9 Isobar P distribution board ensures uniformity across a site and provides the insight to optimise operations.

 

All sites are looking to reduce costs while meeting stringent regulations. Additionally, any refit demands value for money and durability. With that in mind, when installing new fixtures and accessories, products must be considered as a part of a wider electrical ecosystem to enable connectivity and visibility.

 

Design

 

Interior design may not be associated with schools and universities, with practicality and durability typically the modus operandi in that field, but design is a crucial factor for accessibility and compliance and cannot be overlooked. Smart choice in design and colour can go a long way towards making facilities more accessible to users, particularly those with disabilities. As examples, electricians could consider:

 

- Wide rocker switches for easier operation

- Contrasting coloured outboard rockers to improve visibility

- Distinct separation of rockers on a twin socket to simplify operation

- Use of coloured pull cords

 

Have you had any experience with working on educational sites? Do you have any further advice? Please let us know in the comments.

 

 

2 Comments
Esperanto
Ensign

Hello, 

 

Do you have a Part M range?

 

Thanks !

Espé

VictoriaSwift
Lieutenant JG

Hi @Esperanto 

You can find out about our Part M range here: