Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
71208members
324697posts

SI & Cybersecurity Solutions Provider Serve Petrochemical Company

Mahendra
Lieutenant Lieutenant
Lieutenant

SI & Cybersecurity Solutions Provider Serve Petrochemical Company

03_Joint Solution_story.jpg

Case study

 

The challenge

 

Base Sistemas (Certified Alliance SI from Spain) needed a cybersecurity solution for a large petrochemical client in Spain. 

 

The solution

 

Looking for a cybersecurity solutions provider to partner with, SI Base Sistemas posted the petrochemical company's cybersecurity problem in the Exchange Community. Several offer providers - including Enigmedia, an Exchange partner in the domain of cybersecurity - responded with links to their offers in Exchange Shop

 

Enigmedia’s Mercury cybersecurity offer was selected by BaseSistemas as the best solution for the end user, offering benefits including:

 

 Non-intrusive installation

 Plug-and-play deployment (zero-touch provisioning)

 Near-zero latency (less than 2 milliseconds)

 Secure communication even if the WiFi network becomes unsecure

 Data on air protected with encryption and authentication

 

Partnership results

 

The cybersecurity solution from Enigmedia has been accepted by Base Sistemas and the project has progressed into the execution phase.

 

 

Exchange's role

 

Through Exchange, Enigmedia's Mercury cybersecurity solution was discoverable by Base Sistemas, Certified Alliance system integrator. The two companies contacted each other through Exchange, eventually leading to a transaction off the platform.

 

 

Video testimonial

 

Watch the testimonial from Gerard Vidal, CSO at Enigmedia, speaking about his experience using Exchange:

 

 

 

Thanks to Exchange, the procurement process is reduced in just a few clicks.”

–Gerard Vidal, Chief Scientist Officer, Enigmedia