Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
71310members
325014posts

SCADA Integration of Distributed Substations via IEC61850

HMS-Networks
Crewman
Crewman

SCADA Integration of Distributed Substations via IEC61850

03_SCADA_story.jpg

 

A major international airport in Germany needed to upgrade its privately managed power grid. The grid has energy requirements equivalent to a city of 150,000 people, and is managed from a central location. 

 

Customer challenges

 

  • 6 substations distributed over 25 square kilometers

  • Over 100 types of equipment with different protocols

  • Availability and security both of critical importance

  • Limited experience and knowledge of IEC 61850

 

The solution: HMS & EcoStruxure

 

The customer decided to use Ixxat SG-gateways with IEC 61850 connectivity from HMS Networks to establish connections among the equipment, as well as with the central monitoring room. The solution included:

 

  • MiCOM Protection Relays in Modbus-RTU

   Third-party sensors, actuators, or Genset controllers

   Ixxat SG-gateways by HMS Networks 

  • EcoStruxure™ Power Operation (previously Power SCADA Operation)

 

Customer benefits

 

   Fast implementation, thanks to ease of use of Ixxat SG-gateways 

  Simple system with 1 SCADA and 1 gateway type to connect multi-vendor equipment running different protocols

  High security of IEC 61850 for critical application

 

 

Explore EcoStruxure™ Power Operation