Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
71376members
325207posts

Downtime-free operations for bank datacenter – Power Monitoring Expert and Stratus® everRun®

Stratus
Commander
Commander
0
1025

Downtime-free operations for bank datacenter – Power Monitoring Expert and Stratus® everRun®

09_Bank Datacenter_story.jpg

 

Find out how Stratus everRun Enterprise and EcoStruxure Power Monitoring Expert helped a bank datacenter prevent system downtime and data loss.

 

Our Technology Partner

Stratus logo.png

 

 

 

 

 

Customer challenges

For banks to ensure efficient and reliable operations, their datacenters serve a mission-critical function. That's why they rely on advanced Power Control & Monitoring Systems for their facility's electrical network.

 

In case of power loss, basic redundancy enables a quick recovery of operation, but the loss of data can severely impact the customer's ability to track down failure root cause and assess the full impact of the power loss.

 

Since banks process high-volume transactions requiring a high-granularity data collection rate, the customer needed a continuous availability solution that prevents system downtime and data loss from happening.  

 

 

The Solution

To keep the power monitoring systems of the customer up and running at all times, the customer decided to combine EcoStruxure Power Monitoring Expert & Stratus everRun Enterprise

 

The customer installed:

  • EcoStruxure Power Monitoring Expert
  • Stratus everRun Enterprise
  • 2 Intel® x86 servers running Microsoft® Windows® or Red Hat® Linux® and Microsoft SQL Server
  • Over 500 metering devices for critical equipment such as Switchboards, Generators, IT Loads, and more

 

Servers are synchronized via a virtualization platform that pairs protected virtual machines together to create a single operating environment with full redundancy of all underlying hardware and data. If one physical machine fails, the power monitoring software will continue to run on the other physical machine without any interruptions or data loss.

 

Stratus_PME_Bank_Datacenter.JPG

 

 

The Results

 

“Stratus everRun Enterprise enables us to provide customers with complete peace of mind with regard to the availability and integrity of their essential billing data.” - Switchgear Manufacturer

 

  • Bank customers rely on Power Monitoring solution for uninterrupted service.
  • Installation without modification to Power Monitoring Expert
  • Quick single-disc installation and creation of a single operating environment with applications co-existing on two virtual machines.
  • Stratus Support center continuously monitors the systems remotely, and automatically sends notifications if a fault should occur.

 

Learn more about EcoStruxure Power Monitoring Expert & Stratus everRun Enterprise