Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
71297members
324975posts

Connecting BMS with third-party DCIM system for improved efficiency

mike_meirovitz
Lt. Commander
Lt. Commander
0 Likes
0
244

Connecting BMS with third-party DCIM system for improved efficiency

02_Server to Connect BMS_story.jpg

 

Our Technology Partner

_controlsee logo M_72dpi.png

 

Our EcoXpert Partner

TACS.png

 

Customer challenge

 

When the system integrator decided to use a 3rd party DCIM system, he needed to find a scalable solution to allow sharing between EcoStruxure™ Building Operation and the DCIM system.

 

 

The solution

 

The datacenter had previously been equipped with EcoStruxure’s building management solution: EcoStruxure™ Building Operation (EBO), so the system integrator was able to leverage the Smart Connector framework to make the third-party DCIM system interface seamlessly with EBO using OPC Protocol.

 

The server the SI chose was Control See’s OPC Server for Building Operations. It was configured to receive EBO values in real-time into their DCIM system.

 

The OPC server for Building Operations discovers all EBO and connected controllers' points and allows any 3rd party OPC UA or DA client software to browse and select any point that is required by the 3rd party system. EBO Values are pushed to the OPC client software on change. This guarantees high performance of the OPC server and the EBO system. 

 

 

Customer benefits

 

By using Control See’s pre-validated EBO-OPC Server for Building Operations – which utilizes Schneider Electric’s SmartConnector System – both the datacenter and the system integrator benefited from:

 

  • A fast engineering & implementation phase
  • A reliable interface between EBO and any OPC-enabled system.
  • A scalable solution means to easily connect hundreds of EBO values into the DCIM system.

 

EcoStruxure_Scheme1.png

 

 

Testimonial

 

Works as a charm!" – Chris Leijtens, Sr. System & Architecture Engineer - Europe Operations, Schneider Electric, Netherlands

 

 

Explore Control See's EBO-OPC Server for Building Operations

 

Watch Control See’s Webinar How to make you building smart with OPC Connectivity