Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
72193members
327306posts

Two major food manufacturing trends to watch in 2020

MClotteau
Lt. Commander Lt. Commander
Lt. Commander
0
30942

Two major food manufacturing trends to watch in 2020

As we begin to wrap up Q1 2020, I thought it would be interesting to examine the six major food trends that Food Dive believes will have a major impact in 2020. While all these trends are of interest, some are incidental to F&B manufacturing. These trends are less likely to directly affect the plant floor. For instance, the increased prevalence of science-based foods such as cell-cultured meat and plant-based meat, while interesting, is not yet at the scale where manufacturers outside of those specialty areas need to be concerned about the implications. Others, such as an increased use of botanicals, growing demand for “comfort food” and increased adoption of Asian and Middle Eastern flavors are potentially more impactful depending on the specific products that a manufacturer delivers.

 

However, there are two food manufacturing trends that will be extremely important for F&B manufacturers across a variety of markets and end-users – sustainability and transparency.

 

Get help from our Experts to solve your Food & Beverage challenges
 

food-and-bev-ask-question-img_w-btn.png

 

Commitment to environmental sustainability

Perhaps the most significant trend is sustainability. Beyond consumers looking for brands that share their commitment to environmental sustainability, are underlying drivers of food production and food traceability; water, power, both of which are already under pressure in high population growth regions. This means optimizing energy and water consumption is extremely important to just limit environmental impact, but also to ensure future operations. 

 

Digital energy management allows users to correlate energy data with production and process information into actionable metrics and KPIs, allowing operators to make the optimal adjustments to improve energy efficiency. By doing so, companies can continuously improve their sustainability. They can also improve operational efficiency by correlating production events with unusual energy usage patterns or variation in energy consumption. This also helps to improve profitability, because energy is one of the highest costs of F&B manufacturing.

 

UpdatedEnergyManagement_image.jpg

 

                          

Consumer trust is built with product transparency

The second trend is transparency. Food Dive states of the transparency movement, “Recently, it has extended beyond [clean] labels to include product traceability as shoppers grow more interested in where their food comes from and how it was handled along the supply chain.” Consumers are now demanding to know more than ever about how their food was grown, handled, shipped, produced and packaged. This makes transparency one of the most important food manufacturing trends to building consumer trust. Digital transformation of inventory and production operations allows complete end-to-end traceability from receiving materials to shipping completed products, enabling companies to provide the complete traceability consumers demand.

 

This also extends to ensuring products are properly labeled. Mislabeled products and undeclared allergens are the leading cause of recalls. 100% label checks help to reduce the risk of recall and ensure the right product is in the right packaging.

 

 

-----------------------

 

Originally published on SE Blog