Steps leading up to problem:
1) Bring in script block
2) Paste normal code (By default, contains the line E fall thru routine)
3) Compile
4) Save to station
5) Save to controller
6) View workspace
7) Set "Should Poll"
"Should Poll was used for instant verification, it wasn't involved with
causing the halt. You'll get the same result either way.
Program state shows "Halted"
Reliability shows "Configuration Error"
If you try to set Restart to true, or set the Program Change to
any of the other settings, it has no effect to get the script running.
If you "download all objects" it works perfectly. Nothing new was
connected to the block after first creating it and should have worked
right away from the get-go.
Shouldn't the Restart setting allow the script to restart just like in EBO?
Do you just have to do a "download all" to get new scripts working
that you bring in and no other method works to bring them in uniquely?