When interrogating a block after the programming stage is completed,
I tend to pay more attention (and time) looking at the live values and
diagnostics that the block is producing for troubleshooting or for service
support.
In the Script Block properties page, I was wondering if it would be more
beneficial to have the current values of the input/outputs, public numerics,
current line, line start time, TS,TM, TH,TD, scan values near the top of the
arrangement?
Perhaps a views/diagnostics screen all of it's own, similar to Continuum's
script runtime tab?
The block itself can have pin slots selected to show this, but to keep the block
as small as possible, the properties page would really be the catch-all to
troubleshoot script related problems