A new version of the SmartX engineering Module for Niagara is available for testing and has been posted to the box folder.
This version has removed the special MPX network and you are now able to discover SmartX devices from the regular BACnet network.
You should start with a new station. Install the modules like normal, but you will not have to create any special network. Navigate to the BacnetNetwork and then choose the Schneider Device Manager. That will invoke the Network Services that will allow you to engineer like you could in the MPX network before.
We are aware of a few defects. For instance, count Up and Count Down blocks do not function properly. And the latch block does not update if using float data. We will add any other known issues as we find them.
Version 8