With the time change this past sunday, my 2 panels today were now an hour ahead
which allowed me to try a few tests. The Device Object under the Config folder showed
me that this is the case. I did a fresh "download all" to see if the time would sync. It stayed
the same and then i went to the MPX Bacnet Network and saw the TimeSync button as shown
in the picture below. I did that and chose to send the time to all networks. It then changed the
time in the panels.
Question is.... Shouldn't a "download all" be able to have the innate ability of synching the time
of the panel against the time of your station or jace during that process?