I have an MPC-24A. I upgraded the firmware to 3.02.02.10022 and set a static IP address.
I then initialize the controller through the JACE.
I added the controller to the JACE and did a download all. This was completed successfully.
I added a Binary Input from the palette. This was created successfully.
When I click to download all again it fails.
Below are screenshots of the setup, Job Log, Application Director.
Any help is appreciated. Thanks.
Dan,
I'm going to link my post to yours to keep traction on the Jace8000 issue
Jace8000 Hosting an MPX problem (Build 23)
I'm curious if you were to create points in the MPC-24 with the Supervisor
then unhost it. Bring it into the Jace and then do an "Upload All"
In my case i can bring in everything from the Jace's point of view that was
created earlier by the Supervisor and even download it again with the Jace.
As soon as i would create a new point from the Jace's point of view, it would
create successfully, but not download.
After having the issue I found your post and it seems like the same issue. I recently got a new laptop, so it's not licensed for the SmartX. I'll see if I can get it licensed to run the test you did for the Supervisor. Thanks.
Discuss challenges in energy and automation with 30,000+ experts and peers.
Find answers in 10,000+ support articles to help solve your product and business challenges.
Find peer based solutions to your questions. Provide answers for fellow community members!