In EBO when you write a script, you usually compile the script so that the
inputs/outputs can show up correctly in the Initial Values section. After that
you can change the types to float, integer, Boolean, also change the units and
initial values. It required another compile after that before you leave the editor.
For the MPX script editor, I can change these values and send to station, come
back to the script editor and they still show up. Is it best practice or still mandatory
to perform a new compile when changing these settings similar to EBO, or doesn't
it matter in this case and you are allowed to just send to station if there were no
actual script changes made in the document?