Schneider Electric support forum about SmartConnector applications for integration of other building management systems (BMS) into EcoStruxure Building Operation.
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
2024-03-2809:36 AM
as-p-NTP
There is an error in the AS-P time. After setting the internal network NTP server, the time cannot be synchronized. The EBO server time is correct,What parameters do I need to set on the AS-P to synchronize the time of the EBO server, or how do I set the time of the AS-P server synchronizing with the internal NTP server. Thank you!