Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
80721members
346686posts

Bulk Retrieve - not supported with EWS REST Provider

SteveGregory
Commander Commander
Commander

Bulk Retrieve - not supported with EWS REST Provider

Are there any plans to make features like Bulk Retrieve available in the EwsRest provider, like they are in the SboRest provider? These sorts of requests can make third party integrations much easier as they don't have to work their way through the tree to discover all the relevant points. I would really like to see things like GET /Values and GET /Trends work with the EwsRest provider.

Attachments
Tags (1)
3 Replies 3
ardak
Commander Commander
Commander

Re: Bulk Retrieve - not supported with EWS REST Provider

Hi Steve,

 

Bulk retrieve will never be available in the EWS provider, since EWS unfortunately doesn't support it.

 

We are looking into other ways of improving the REST gateways capabilities, hopefully including some kind of bulk retrieve capability.

 

BR

Armend

Tags (1)
SteveGregory
Commander Commander
Commander
0 Likes
1
272

Re: Bulk Retrieve - not supported with EWS REST Provider

Hi Armend, 

 

Thanks for that info.

 

Are there any plans to update the SboRest provider which did support it?

 

Steve

Tags (1)
ardak
Commander Commander
Commander
0 Likes
0
258

Re: Bulk Retrieve - not supported with EWS REST Provider

That is one of the options that we are looking into. Todays implementation has some drawbacks since it's tied to one version of EBO, which even if updated, would have compatibility problems both backwards and in the future. We are looking into ways of mitigating this.

 

BR

Armend

Tags (1)