Segment Specializations Forum
The Segment Specialization forum is your place to ask questions, find solutions, share knowledge, and submit ideas related to specific market segments, such as, Hotels, Healthcare, Retail, Real Estate, or Life Sciences.
Link copied. Please paste this link to share this article on your social media post.
We're also very excited to announce that in addition to the documented 105x105 panels, you will now have the option for a second size: 95x95 across the entire range.
And again, these are all Modbus RTU compatible with self-discovery and configuration when using the HRC.
NOTE: GTP are not available in all regions. Please contact your Channel Manager to see if they are available in your region.
Link copied. Please paste this link to share this article on your social media post.
FYI, there may be some issues with suitable wall boxes when you try to localise the product.
1/ AU / NZ region has no standard in-wall metal wall boxes to suit this product with a 60.3 mm mounting centres.
2/ We used to carry 60.3 mount surface mounted boxes for export to UK market but those were surface mount PVC style box. E238 (single gang), ET238 (double gang),
so those would not be suitable for flush mounting regardless.
3/ I once imported in the UK wall boxes from our sister company GET (UK based) part # SB471 (single gang) and SB472 (double gang). We used them for
Lexcom audio ( now deceased product line since approx 2012 in AU market).
4/ Fairly sure that AU region has no fire-rated wall box to suit these products @ 60.3 mounting centres. (EPIC boxes are odd sizes)
So mounting within a room is limited to non-fire rated walls. Wall boxes for Fire-rated wall installation are "prescribed articles" in AU.
Even if you made a wallbox to suit, it would need to be submitted to local testing authorities for approvals testing.
Not cheap for the testing costs either.
Link copied. Please paste this link to share this article on your social media post.
I need intergrated Glass Touch Panels with AS-P.
Do you have modbus register of All Glass Touch Panels.
Thanks.
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.